SNVU888 March 2024
This section describes how to set up the LP5811-10EVM properly. Items from the following list are required to begin evaluating the LP5811/LP5810:
In the default jumper setting, the board can be evaluated by USB2ANY power directly and does not need an external power supply. Setup connection is demonstrated in Figure 2-1. The setup procedure is as follows: