SPNA248 March   2021 TM4C1292NCPDT , TM4C1292NCPDT , TM4C1292NCZAD , TM4C1292NCZAD , TM4C1294KCPDT , TM4C1294KCPDT , TM4C1294NCPDT , TM4C1294NCPDT , TM4C1294NCZAD , TM4C1294NCZAD , TM4C1299KCZAD , TM4C1299KCZAD , TM4C1299NCZAD , TM4C1299NCZAD , TM4C129DNCPDT , TM4C129DNCPDT , TM4C129DNCZAD , TM4C129DNCZAD , TM4C129EKCPDT , TM4C129EKCPDT , TM4C129ENCPDT , TM4C129ENCPDT , TM4C129ENCZAD , TM4C129ENCZAD , TM4C129LNCZAD , TM4C129LNCZAD , TM4C129XKCZAD , TM4C129XKCZAD , TM4C129XNCZAD , TM4C129XNCZAD

 

  1.   Trademarks
  2. Introduction
    1. 1.1 License
    2. 1.2 IwIP Version
    3. 1.3 lwIP Customization
    4. 1.4 IwIP API
      1. 1.4.1 TCP RAW APIs
      2. 1.4.2 UDP RAW APIs
    5. 1.5 lwIP Development Home Page and Support
  3. Application Examples
  4. Application Setup
    1. 3.1 Hardware Setup
    2. 3.2 Software Tools
  5. Download and Import the Ethernet examples
  6. Enet_tcpecho_server_lwip Example Overview
    1. 5.1 Build and Flash the Program
    2. 5.2 Check and Program the MAC Address
      1. 5.2.1 Using The LM Flash Programmer
      2. 5.2.2 Using the CCS
      3. 5.2.3 Using Uniflash
    3. 5.3 Configure the Terminal Window
    4. 5.4 Run the enet_tcpecho_server_lwip Example
  7. Enet_tcpecho_server_static_ip_lwip Example Overview
    1. 6.1 How to Configure lwIP for Static Address
    2. 6.2 Run the enet_tcpecho_server_static_ip_lwip Example
  8. Enet_udpecho_server_lwip Example Overview
    1. 7.1 Run the enet_udpecho_server_lwip Example
  9. Enet_dns_lwip Example Overview
    1. 8.1 How to Configure lwIP for DNS
    2. 8.2 How to View the DNS Traffic on Wireshark
    3. 8.3 Run the enet_dns_lwip Example
  10. Enet_sntp_lwip Example Overview
    1. 9.1 Run the enet_sntp_lwip Example
  11. 10Enet_tcpecho_client_lwip Example Overview
    1. 10.1 Configure the Server IP Address
    2. 10.2 Configure the SocketTest Server and Run the enet_tcpecho_client_lwip Example
    3. 10.3 Wireshark Capture for enet_tcpecho_client_lwip Example
  12. 11Enet_adcsensor_client_lwip Example Overview
    1. 11.1 Run the adcsensor_client_lwip Example
  13. 12Enet_udpecho_client_lwip Example Overview
    1. 12.1 Run the enet_udpecho_client_lwip Example
  14. 13References

Software Tools

Several tools are used to facilitate the debugging and testing of the application examples:

  • CCS. The IDE tool is used to debug the target device and build the application examples. The CCS v10.1.1 and the TI v20.2.4.LTS compiler is used for this application report.
  • SocketTest. A free small software tool that tests any server or client that uses TCP or UDP protocol to communicate.
  • Wireshark. A free packet analyzer that is used for network troubleshooting and analysis in this application report.
  • Terminal Emulator. The application examples use the terminal window to display its outputs. Any serial terminal emulator may be used. CCS has a built-in terminal emulator which is used in this application report. The terminal window can be invoked with “View” -> “Terminal”.