SPNA248 March 2021 TM4C1292NCPDT , TM4C1292NCPDT , TM4C1292NCZAD , TM4C1292NCZAD , TM4C1294KCPDT , TM4C1294KCPDT , TM4C1294NCPDT , TM4C1294NCPDT , TM4C1294NCZAD , TM4C1294NCZAD , TM4C1299KCZAD , TM4C1299KCZAD , TM4C1299NCZAD , TM4C1299NCZAD , TM4C129DNCPDT , TM4C129DNCPDT , TM4C129DNCZAD , TM4C129DNCZAD , TM4C129EKCPDT , TM4C129EKCPDT , TM4C129ENCPDT , TM4C129ENCPDT , TM4C129ENCZAD , TM4C129ENCZAD , TM4C129LNCZAD , TM4C129LNCZAD , TM4C129XKCZAD , TM4C129XKCZAD , TM4C129XNCZAD , TM4C129XNCZAD
The enet_udpecho_client_lwip example is a client application using UDP protocol. It is similar to the server example in terms of the APIs as depicted in the UDP flowchart in Figure 1-2. The difference is that the client needs to call the udp_connect() to first associate the PCB with the remote address. This example will use udp_send() to send a greeting message “Hello! Greeting from EK-TM4C1294XL LaunchPad\n\r” to the remote server. It will then echo anything that it receives from the server.