SPNU118Z September 1995 – March 2023 66AK2E05 , 66AK2H06 , 66AK2H12 , 66AK2H14 , AM1705 , AM1707 , AM1802 , AM1806 , AM1808 , AM1810 , AM5K2E04 , OMAP-L132 , OMAP-L137 , OMAP-L138 , SM470R1B1M-HT , TMS470R1A288 , TMS470R1A384 , TMS470R1A64 , TMS470R1B1M , TMS470R1B512 , TMS470R1B768
The --generate_dead_funcs_list option creates a list of functions that are never referenced (dead) and writes the list to the specified file. If no filename is specified, the default filename dead_funcs.xml is used. The syntax for the option is:
--generate_dead_funcs_list=filename
Refer to the ARM Optimizing C/C++ Compiler User's Guide for details on the --generate_dead_funcs_list option and the corresponding --use_dead_funcs_list option.