SPRABN2A March 2019 – December 2019 AM3352 , AM3354 , AM3356 , AM3357 , AM3358 , AM3358-EP , AM3359
Be sure to check the device-specific TRM uses for warm reset. The warm reset signal should be used as an input (for example, connected to a push button) or output (to reset external devices during a POR). It cannot be used for both because of an errata with the clocking of the debounce circuitry.