SPRAC71B February 2019 – October 2023
The R_C28X_NONE relocation type performs no operation. It is used to create a reference from one section to another, to ensure that if the referring section is linked in, so is the referent section.
R_C28X_PREL31 is used to encode code addresses in exception handling tables. See Section 9.2.