The QepOnClb implementation uses the
following C2000 resources:
- C28x CPU
- Initializes the QepOnClb
interface, configures the CLB, input/output XBARs and GPIOs.
- Configures the CLB to
implement a basic QEP decoder module in quadrature-count mode.
- Configurable Logic Block (CLB)
type 1 or later
- 1 CLB tile. Refer to Section 5.4 for specific CLB blocks used.
- 32-bit QEP position counter
with programmable max position.
- QEP direction decode from
QEP-A/B
- QEP state transition error
detection
- Latch of the position counter
on QEP-I
- Device interconnect (XBARs)
- Input and output XBARs are
used to route signals to the CLB as applicable.