SPRAC77E January 2022 – February 2022 TMS320F28379D , TMS320F28379D-Q1 , TMS320F28379S
The following watch variables provide pass/fail information:
The angle of the absolute position is compared to the angle corresponding to the eQEP position counter (QPOSCNT). If the difference is less than a specified threshold, then passCount is incremented. If not, then failCount is incremented. The maximum difference is logged in deltaMax.