Install required software to build and run the PTO examples:
- Install Code Composer Studio v11.0.0 or later, if it is not already installed on the PC
- Install C2000WARE-MOTORCONTROL-SDK v4.00.00.00 or later, if it is not already installed on the PC
Note: To build the examples, only the above software is required. To re-build the CLB-based libraries, the CLB Tool is also required. This tool is included in Code Composer Studio (sysconfig) and the C2000Ware sub-component of the SDK (support utilities). To run CLB-based simulations requires installation of additional tools which are documented in the
CLB Tool User's Guide.