The PTO-QepDiv operation has the following
usage limitations:
- The QepDiv interface implements division factors of /1, /2, /4, /8, ….. up to /1024
and /2048.
- The maximum frequency of the input signals (QEP-A and QEP-B) is
limited to 5 MHz.
- The index pulse is generated on the index output when a rising edge
is detected on the index input signal.
- The width of the index pulse can be user defined. See the
pto_qepdiv_config
function and the corresponding example
provided in C2000Ware MotorControl SDK.
- The divider values work as follows:
- The frequency of the output QEP-A or QEP-B = frequency of
input QEP-A or QEP-B / (2 × divider)