The PTO-PulseGen operation has the
following usage limitations:
- The minimum number of cycles must be 1000 cycles for the PTO period
(at 200-MHz system clock, this corresponds to 10 µs [for example, 100 KHz]).
- The number of cycles must be between 40% to 60% of the PTO period
for the interrupt time to avoid conflicts with PTO updates.
- The maximum frequency of the PTO-PulseGen output is 5 MHz at a
200-MHz CPU CLK. See the example provided in C2000Ware MotorControl SDK.