DC blocking capacitors are required for data lanes and should be implemented on the RX end.
The SerDes receiver includes a 100 Ω internal termination, so an external 100 Ω termination is not needed.
If both of the SGMII interfaces are not used, the SGMII regulator power pin (VDDR3_SGMII) must still be connected to the correct supply rail with the appropriate decoupling capacitance applied.
Both SRIO and SGMII interfaces must be unused in order to pull-up the unused clock signal (SRIOSGMIICLK) for devices that have these combined.