SPRACM8A June 2019 – January 2021 OMAP-L132 , OMAP-L132 , OMAP-L138 , OMAP-L138 , TMS320C6742 , TMS320C6742 , TMS320C6746 , TMS320C6746 , TMS320C6748 , TMS320C6748
Code Composer Studio is a trademark of Texas Instruments Incorporated.
Microsoft are registered trademarks of Microsoft Corporation in the United States and/or other countries.
Arm is a registered trademark of Arm Limited (or its subsidiaries) in the US and/or elsewhere.
All trademarks are the property of their respective owners.
This application report describes the boot process of the OMAP-L138 Arm® + DSP SoC. The content here also applies to the AM1808 and C6748 devices, unless otherwise specified.
There are two types of reset:
It is important for the device to experience a POR when initially powered up. This will clear the emulation and PLL logic, as well as latch the boot pins correctly. Therefore, make sure TRST is externally pulled down on your board. Not doing so can be the cause of many boot related problems.
When the device is held in reset, all device I/Os are internally pulled down.
For the boot and configuration pins, if they are both routed out and 3-stated (not driven), it is strongly recommended that an external pullup/pulldown resistor be implemented. Although, internal pullup/pulldown resistors exist on these pins and they may match the desired configuration value, providing external connectivity can help ensure that valid logic levels are latched on these device boot and configuration pins. In addition, applying external pullup/pulldown resistors on the boot and configuration pins adds convenience to the user in debugging and flexibility in switching operating modes.
For details on how to choose values to oppose the internal pullup/pulldown resistors, see the Pullup/Pulldown Resistors section of the OMAP-L138 C6000™ DSP+ ARM® Processor Data Manual.
On the rising edge of RESETn, the following steps will occur:
This only occurs when coming out of a POR, as the boot pins will not be relatched after a warm reset.