SPRACN3 September 2019 66AK2E05 , 66AK2H06 , 66AK2H12 , 66AK2H14 , 66AK2L06 , AM5K2E02 , AM5K2E04
SPI boot is a general-purpose boot mode in which the Boot ROM configures the PLL in bypass mode. The Boot ROM loads the image from the base of the SPI NOR flash. In the multi-stage boot example, the first stage loads the boot parameter table that forces the Boot ROM to configure the PLL and load the seconds stage at 100 Khz. The second stage is loaded at an offset of 0x1000 in the SPI NOR Flash.