SPRACU1A October 2020 – June 2021 AM2431 , AM2432 , AM2434 , AM6411 , AM6412 , AM6421 , AM6441 , AM6442
As with CK and ADDR_CTRL, a reasonable trace route length is to within a percentage of its Manhattan distance. DQLMn is defined as DQ Longest Manhattan distance n, where n is the byte number. For a 16-bit interface, there are two DQLMs, DQLM0 and DQLM1.
Given the DQS, DQ, and DM pin locations on the processor and the DDR4 memories, the maximum possible Manhattan distance can be determined given the placement. It is from this distance that and upper limit on the lengths of the transmission lines for the data bus can be established. Unlike the CACLM, there is no margin added to the DQLMn limits. These limits are simply the sum of the horizontal and vertical distances for the longest pin to pin route for that byte group.