SPRACU1A October 2020 – June 2021 AM2431 , AM2432 , AM2434 , AM6411 , AM6412 , AM6421 , AM6441 , AM6442
Use additional bypass capacitors if the return current reference plane changes due to DDR signals hopping from one signal layer to another, resulting in the reference plane changing from VDDS_DDR to VSS. The bypass capacitor here provides a path for the return current to hop planes along with the signal. Use as many of these return current bypass capacitors as possible – up to one per signal via. Because these are returns for signal current, the via size for these bypass capacitors can be the smaller via used for signal routing.