SPRACU5C June 2021 – September 2023 AM2431 , AM2432 , AM2434 , AM6411 , AM6412 , AM6421 , AM6422 , AM6441 , AM6442
It is recommended to connect the OSPI (processor) to a single memory device. In case the OSPI is interfaced to multiple memory devices, the interface would create a split data bus which could severely degrade signal integrity at high speeds. For accessing OSPI at high speeds, a point-to-point data bus is recommended.