SPRACU5C June 2021 – September 2023 AM2431 , AM2432 , AM2434 , AM6411 , AM6412 , AM6421 , AM6422 , AM6441 , AM6442
When using NAND / NOR flash with GPMC, many of the memories interfaced over GPMC may not have the reset signal.
It is optional to use the reset signal. In case reset pin is available, review the reset requirements and connect the reset pin to the relevant reset source.