All trademarks are the property of their respective owners.
Cameras are key component of vision based systems in industrial and automotive markets. The number of cameras, frame rates and resolutions of those cameras have been increasing significantly in industrial and automotive applications including machine vision, robotics, video surveillance, Advanced Driver Assistance Systems (ADAS), and so forth. It is critical for an application processor used in such applications to capture and process those camera inputs including raw input. Jacinto 7-based high-performance heterogenous application processors, including TDA4VM and DRA829 [1] and [2], provide capabilities to capture and process multiple camera inputs to optimize performance, power and memory throughput.
Jacinto 7 camera and capture system is Texas Instruments’ 7th generation imaging subsystem (ISP) built on the top of more than 20 years of innovation in multiple SoC families deployed in millions of products. Some of the differentiated features include: