SPRAD06B March 2022 – November 2024 AM620-Q1 , AM623 , AM625 , AM625-Q1
Figure 2-2 shows the schematic connections for a dual rank,16-bit interface using two x8 devices.
It is also possible to use memory devices with two dies in one package to achieve higher density designs. The connection would look similar to Figure 2-2, except the two x8 memories are in one package, and thus VTT implementation is not necessary. Ensure to connect BG[1:0] when using these devices, as the internal implementation is still using two x8 memories.