SPRAD06B March 2022 – November 2024 AM620-Q1 , AM623 , AM625 , AM625-Q1
Figure 3-2 shows the required placement for the processor and the LPDDR4 device. The dimensions for this figure are defined in Table 3-3. The placement does not restrict the side of the PCB on which the devices are mounted. The ultimate purpose of the placement is to limit the maximum trace lengths and allow for proper routing space.
Number | Parameter | MIN | MAX | UNIT |
---|---|---|---|---|
1 | x1 | 2000 | Mils | |
2 | y1 | 1000 | Mils |