SPRAD06B March 2022 – November 2024 AM620-Q1 , AM623 , AM625 , AM625-Q1
Use additional bypass capacitors if the return current reference plane changes due to DDR signals hopping from one signal layer to another, resulting in the reference plane changing from VDDS_DDR to VSS. The bypass capacitor here provides a path for the return current to hop planes along with the signal. Use as many of these return current bypass capacitors as possible – up to one per signal via. Because these are returns for signal current, the via size for these bypass capacitors can be the smaller via used for signal routing.