SPRAD21F May 2022 – November 2024 AM620-Q1 , AM623 , AM625 , AM625-Q1 , AM625SIP , AM62A3 , AM62A3-Q1 , AM62A7 , AM62A7-Q1 , AM62P , AM62P-Q1
When external inputs drive the boot mode configuration, stabilize the boot mode configuration inputs during the processor POR (cold reset).
When using an Ethernet boot and a Reduced Gigabit Media Independent Interface (RGMII), implement an EPHY into the design that starts RGMII_ID mode on the EPHY RX data path and disables RGMII_ID mode on the TDn data path (the processor implements RGMII_ID on the TDn outputs). The processor ROM does not enable or disable RGMII_ID mode on attached EPHYs programmatically. Typically, RGMII_ID setting is accomplished via pin strapping on the EPHY.
Select a EPHY with the capability to set the RGMII internal delay through a pin strap, see the processor-specific SK. For more information, see the advisory i2329 MDIO: MDIO interface corruption (CPSW and PRU-ICSS) of the processor-specific silicon errata.