SPRAD21F May 2022 – November 2024 AM620-Q1 , AM623 , AM625 , AM625-Q1 , AM625SIP , AM62A3 , AM62A3-Q1 , AM62A7 , AM62A7-Q1 , AM62P , AM62P-Q1
The section has been added to the application. All the relevant peripheral or power sections in the application note includes checklist categorized as General, Schematic Review, and Additional. User can use the checklist to do a self-review of the custom board schematics to minimize possible errors that may cause functional or performance issues resulting in increased board bring-up and testing time.