SPRAD24 august   2023 AM2631 , AM2632 , AM2632-Q1 , AM2634 , AM2634-Q1 , AM263P4 , AM263P4-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
    1. 1.1 Key System Specifications
  5. 2AM263x Overview
    1. 2.1 AM263x Control Card and Traction System Framework
  6. 3Guide to Running TIDM-02014 Traction Inverter
    1. 3.1 Software Set-up
      1. 3.1.1 Code Composer Studio Project
      2. 3.1.2 Software Structure
    2. 3.2 Create Real Time Debug Interface
      1. 3.2.1 Confirm CCS Features
      2. 3.2.2 Create Target Configuration File
      3. 3.2.3 Add Serial Command Monitor Software
      4. 3.2.4 Launch Real Time Debug
    3. 3.3 Running the Code
      1. 3.3.1 Project Setup
      2. 3.3.2 Running the Application
    4. 3.4 Get Samples From ADC and Read Samples Through CCS
      1. 3.4.1 Register and Enable Interrupt
      2. 3.4.2 Add Log Code to Read Samples in Graph at Fixed Rate
      3. 3.4.3 Read ADC Samples in Expression and Graph Windows
    5. 3.5 Generate Space Vector PWM and Drive Motor in Open Loop
      1. 3.5.1 Setup SVPWM Generator Inputs
      2. 3.5.2 Read SVPWM Duty Cycles in Graph Window
      3. 3.5.3 Power Up Inverter and Spin Motor in Open Loop
    6. 3.6 Close Current Loop With Mock Speed
      1. 3.6.1 Add Transformations and Read Id-Iq in Open Loop
      2. 3.6.2 Add Controllers to Close Current Loop
      3. 3.6.3 Read Id-Iq to Close Current Loop
    7. 3.7 Add Software Resolver to Digital Converter
      1. 3.7.1 Generate Excitation for Resolver Hardware
      2. 3.7.2 Add Resolver Software
      3. 3.7.3 Read Resolver Software Outputs
  7. 4Brief Guide to Code Migration
    1. 4.1 SDK Resources Overview
    2. 4.2 Code Migration From C28
    3. 4.3 Code Migration From AM24
  8. 5Summary
  9. 6References

Software Set-up

After setting up the traction system as shown in the Figure 2-3, the TIDM-02014 reference design needs the software environment to be set-up to run it. We used Code Composer Studio (CCS) as the integrated development environment for this purpose.

As a first step, please download and install CCS version 12.2.0 or newer that is recommended for this project. CCS User's Guide provides more details about CCS installation and use.

While it is not strictly necessary, establishing a real time debug interface helps a lot in debugging any power conversion application with an MCU. For AM263x, real time debug is enabled by UART connection between CCS and AM263x. The user interfaces of the AM263x control card are shown in Figure 3-1. The details on hardware connection can be found in AM263x Control Card User's Guide. The control card offers both JTAG and UART debugging ports in one USB Micro-B connector. A detailed explanation of creating a target configuration file for the debug ports can be found in the application note AM263x for Traction Inverters. As this application note also covers in detail how to configure control peripherals, interrupts and driver interfaces, we are not repeating those sections here.

GUID-20211120-SS0I-DCT4-7WXT-6XHBSF92QJXW-low.png Figure 3-1 User Interfaces of AM263x Control Card