There are a few things to consider when choosing a flash part for application purposes. This application report covers some of the basic requirements that a specific flash memory must support to be compatible with the AM263x device during both boot operation and application execution.
All trademarks are the property of their respective owners.
The QSPI Flash memory can be utilized two different ways in the user system:
When picking a Flash memory IC, the device must comply with all boot requirements of the system-on-chip (SoC). If the memory is used as boot media, some guidelines must be followed to work efficiently as a storage device during application.
Figure 1-1 depicts the Flash memory organization once the secondary bootloader (SBL) image and valid application image are present.
SBL - Secondary Boot loader
MCU – Microcontroller Unit
QSPI – Quad Serial Peripheral Interface
ROM – Read-only memory
SoC – System on a Chip
SDK – Software Development Package
UART – Universal Asynchronous Receiver-Transmitter