This section details the steps needed
to run the DCAN Flash Kernel on the ControlCard:
- Enter a command with the
parameters as described below:
- Example:
dcan_flash_programmer.exe -d f28003x -k
flash_kernel_ex5_dcan_flash_kernel.txt -a led_ex1_blinky.txt
-v
- After the kernel is downloaded, it moves the application file to flash and
confirms that the application load has completed.
For the LaunchPad, the following steps
must be taken:
- Set LaunchPad SW4 position to OFF
(down). This is done to route the CANTX and CANRX signals to the header instead
of the transceiver.
- Open up a command window and navigate to where dcan_flash_programmer.exe
is.
- Enter a command with the parameters as described below:
- Example: dcan_flash_programmer.exe -d f28003x -k
flash_kernel_ex5_dcan_flash_kernel.txt -a led_ex1_blinky.txt
-v
- After the kernel is downloaded,
it transfers the firmware to flash and confirms that the application load has
completed.