SPRAD59 October   2023 TMS320F280039

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. Introduction
  5. Key Differences Between DCAN and MCAN
  6. Module Initialization
    1. 3.1 DCAN Initialization
    2. 3.2 MCAN Initialization
    3. 3.3 Initialization sequence
    4. 3.4 Code Snippets for Module Initialization
  7. Bit Timing Configuration
  8. Message RAM Configuration
  9. Interrupt handling
    1. 6.1 MCAN Interrupt Sources
    2. 6.2 DCAN Interrupt Handling
    3. 6.3 MCAN Interrupt Handling
  10. Transmitting data
    1. 7.1 Basic Transmission Process
      1. 7.1.1 Transmission with DCAN
      2. 7.1.2 Transmission with MCAN
    2. 7.2 MCAN Vs DCAN Transmit Procedural Differences
    3. 7.3 MCAN Transmit Concepts
      1. 7.3.1 Tx Event FIFO
  11. Receiving Data
    1. 8.1 Introduction to Reception
    2. 8.2 Basic Reception Process
      1. 8.2.1 DCAN Reception
      2. 8.2.2 MCAN Reception
    3. 8.3 Filter Elements
      1. 8.3.1 Filter Element Structure
    4. 8.4 Rx Buffer
      1. 8.4.1 Receiving in Rx Buffer
    5. 8.5 Rx FIFO
      1. 8.5.1 Receiving in Rx FIFO
    6. 8.6 Receiving High Priority Messages
  12. Avoiding network errors
  13. 10References

Introduction

On any given device, C2000 MCUs have typically featured only one type of CAN module. For example, either eCAN or DCAN. When MCAN was introduced in the C2000 family, some MCUs featured both DCAN and MCAN. This necessitated the user to understand and program two completely different types of CAN modules. To eliminate this hardship, MCAN has been chosen as the CAN platform moving forward, since MCAN supports both classic CAN as well as CAN FD. This document lists the primary differences between the DCAN and MCAN modules. It then proceeds to highlight how common operations are done in both modules.

To determine which CAN module is featured in a given C2000 MCU, see C2000 Real-time Control MCU Peripherals Guide.