SPRAD59 October 2023 TMS320F280039
Certain Filter Elements can be configured to treat matching frames as high priority messages. Note that the messages themselves are indisinguishable (identical) from other messages, but the module reads them slightly differently. Messages can only be read from a FIFO in the order in which the messages were received. However, priority messages can be read directly. This is possible because there is a separate register (MCAN_HPMS) that stores information related to the High Priority Message including whether the message is Standard ID or Extended ID, what is the filter index for the matching filter element, in which FIFO the message is stored and the corresponding index within the FIFO.
For more information on how to receive High Priority Messages, please refer to the example available in C2000ware.