SPRAD62 February 2023 F29H850TU , F29H859TU-Q1 , TMS320F280023C , TMS320F280025C , TMS320F280025C-Q1 , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280038C-Q1 , TMS320F280039C , TMS320F280039C-Q1 , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388S , TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
This section discusses the instructions on how to test the Code Composer Studio™ example project provided for the CLB-based TDM-8 example. The example is tested on the F280025C controlCARD (TMDSCNCD280025C). However, the code can be easily ported to any other MCU with support for CLB Types 2 and above.
For test purposes, a separate F28388D MCU is used to generate a test TDM-8 stream using a McBSP port. The F28388D also receives the TDM-8 stream from the CLB and check for errors. An F28388D controlCARD (TMDSCNCD28388D) is used for this test.
In this test, the F28388D is configured for 200MHz operation with the McBSP generating a TDM waveform at 12.5MHz. The F280025C is configured for maximum 100MHz operation.
Figure 3-12 shows the required setup to test the TDM-8 example.