SPRAD62 February 2023 F29H850TU , F29H859TU-Q1 , TMS320F280023C , TMS320F280025C , TMS320F280025C-Q1 , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280038C-Q1 , TMS320F280039C , TMS320F280039C-Q1 , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388S , TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
The output TDM-8 stream signals are connected to the CLB tile boundary outputs using the CLB OUTPUT XBAR and the GPIO OUTPUT XBAR as shown in Figure 3-4.
As previously mentioned, the input BCLK signal must be passed through the CLB tile unregistered (i.e. it is not synchronized to any internal clock) to avoid introducing jitter at the output BCLK signal. Only CLB outputs 4 and 5 can be passed unregistered through the CLB tile. Therefore, CLB output 5 is used for BCLK_OUT. Furthermore, the BCLK signal is brought to the GPIO pin through the GPIO OUTPUT XBAR.