SPRAD66A February   2023  – December 2023 AM62A3 , AM62A3-Q1 , AM62A7 , AM62A7-Q1 , AM62P , AM62P-Q1

 

  1.   1
  2.    AM62Ax/AM62Px LPDDR4 Board Design and Layout Guidelines
  3.   Trademarks
  4. 1Overview
    1. 1.1 Board Designs Supported
    2. 1.2 General Board Layout Guidelines
    3. 1.3 PCB Stack-Up
    4. 1.4 Bypass Capacitors
      1. 1.4.1 Bulk Bypass Capacitors
      2. 1.4.2 High-Speed Bypass Capacitors
    5. 1.5 Velocity Compensation
  5. 2LPDDR4 Board Design and Layout Guidance
    1. 2.1  LPDDR4 Introduction
    2. 2.2  LPDDR4 Device Implementations Supported
    3. 2.3  LPDDR4 Interface Schematics
    4. 2.4  Compatible JEDEC LPDDR4 Devices
    5. 2.5  Placement
    6. 2.6  LPDDR4 Keepout Region
    7. 2.7  Net Classes
    8. 2.8  LPDDR4 Signal Termination
    9. 2.9  LPDDR4 VREF Routing
    10. 2.10 LPDDR4 VTT
    11. 2.11 CK and ADDR_CTRL Topologies
    12. 2.12 Data Group Topologies
    13. 2.13 CK0 and ADDR_CTRL Routing Specification
    14. 2.14 Data Group Routing Specification
    15. 2.15 Channel, Byte, and Bit Swapping
    16. 2.16 Data Bus Inversion
  6. 3LPDDR4 Board Design Simulations
    1. 3.1 Board Model Extraction
    2. 3.2 Board-Model Validation
    3. 3.3 S-Parameter Inspection
    4. 3.4 Time Domain Reflectometry (TDR) Analysis
    5. 3.5 System Level Simulation
      1. 3.5.1 Simulation Setup
      2. 3.5.2 Simulation Parameters
      3. 3.5.3 Simulation Targets
        1. 3.5.3.1 Eye Quality
        2. 3.5.3.2 Delay Report
        3. 3.5.3.3 Mask Report
    6. 3.6 Design Example
      1. 3.6.1 Stack-Up
      2. 3.6.2 Routing
      3. 3.6.3 Model Verification
      4. 3.6.4 Simulation Results
  7. 4Appendix: SOC Package Delays
  8. 5References
  9. 6Revision History

PCB Stack-Up

The recommended stack-up for routing the DDR interface is a ten or twelve layer stack up. However, this can only be accomplished on a board with routing room with large keep-out areas. Additional layers are required if:

  • The PCB layout area for the DDR Interface is restricted, which limits the area available to spread out the signals to minimize crosstalk.
  • Other circuitry must exist in the same area, but on layers isolated from the DDR routing.
  • Additional planes layers are needed to enhance the power supply routing or to improve EMI shielding.

Board designs that are relatively dense may require more layers to properly allow the DDR routing to be implemented such that all rules are met.

All DDR signals must be routed adjacent to a solid VSS reference plane. When multiple VSS reference planes exist in the DDR routing area, stitching vias must be implemented nearby wherever vias transfer signals to a different VSS reference plane. This is required to maintain a low-inductance return current path.

It is strongly recommended all DDR signals be routed as strip-line. Some PCB stack-ups implement signal routing on two adjacent layers. This is not recommended as crosstalk occurs on any trace routed parallel to another trace on an adjacent layer, even for a very short distance. It is recommended to route LPDDR4 signals on PCB layers closer to the SoC within the stackup, giving the signal a shorter travel time through the via. The PCB layers farther from the SoC will have longer travel times through the via, which can increase coupling between vias. Both signal and via coupling can lead to smaller timing margins.

Note a shorter via travel could mean a longer via stub (if using standard drill vias), so that is to be considered as well. Simulation can be used to determine if via stub length is an issue.

PCB material is another important factor. Depending on the design specifics, it may be required to use a higher frequency material such as ISOLA I-Speed or equivalent/better to achieve highest data rates. For supported data rates/speed grades, see the device-specific data manual. Standard FR4 products like 370HR can be used for lower data rates. In specific cases, it is sufficient for higher data rates as well.

Table 1-1 PCB Stack-up Specifications
Number Parameter(6) MIN TYP MAX UNIT
PS1 PCB routing plus plane layers 10 or 12
PS2 Signal routing layers 6
PS3 Full VSS reference layers under DDR routing region (1) 1
PS4 Full VDDS_DDR power reference layers under the DDR routing region (1) 1
PS5 Number of reference plane cuts allowed within DDR routing region (2) 0
PS6 Number of layers between DDR routing layer and reference plane (3) 0
PS7 PCB routing feature size 4 Mils
PS8 PCB trace width, w 3 Mils
PS9 Point-to-Point, single-ended impedance 40
PS10 Point-to-Point, differential impedance 80
PS11 T-Branch, single-ended impedance (5) 35/70
PS12 T-branch, differential impedance (5) 70/140 (7)
PS13 Impedance control (4) Z-10% Z Z+10%
Ground reference layers are preferred over power reference layers. Return signal vias need to be near layer transitions.
No traces should cross reference plane cuts within the DDR routing region. High-speed signal traces crossing reference plane cuts create large return current paths, which can lead to excessive crosstalk and EMI radiation. Beware of reference plane voids caused by via antipads, as these also cause discontinuities in the return current path.
Reference planes are to be directly adjacent to the signal layer, to minimize the size of the return current loop.
Z is the nominal singled-ended or differential impedance selected for the PCB specified by PS9-PS12.
Balanced T traces (also referred to as T-branch traces) are split traces from source to multiple end points. The target impedance of the split trace should be twice that of the non-branched impedance. See routing topologies. The maximum trace impedance is typically limited by the minimum trace width achievable. Reduction of the non-branched impedance may be necessary to maintain the 2:1 trace impedance ratio.
These specifications are to be used as a starting point for designs. It is recommended each design be extracted and simulated to ensure all requirements are met.
These values can be relaxed to 60/120 to facilitate fabrication, but it is recommended to prove eye margins are still adequate with simulations.