SPRAD66B February 2023 – December 2024 AM62A1-Q1 , AM62A3 , AM62A3-Q1 , AM62A7 , AM62A7-Q1 , AM62D-Q1 , AM62P , AM62P-Q1
The methodology for validating the DDR interface is outlined in this section. LPDDR4 interfaces, as defined in the JEDEC specification, uses eye masks defined at a target BER (Bit Error Rate) to determine pass or fail for signal integrity. This is essential to perform channel simulations using IBIS models to generate the signal eye diagrams at the targeted BER. These are introduced for memory interfaces starting from LPDDR4