SPRAD67B December 2022 – September 2024 AM2431 , AM2432 , AM2434 , AM6411 , AM6412 , AM6421 , AM6422 , AM6441 , AM6442
The processor family supports an integrated LDO (SDIO_LDO) to power the SDIO interface IO supply group and SD interface pullups, capable of dynamically switching between 1.8V and 3.3V voltage. The recommended output capacitor must be connected close to the LDO output pin (CAP_VDDSHV_MMC1). For guidance on recommended capacitance and connection, refer to the Power Supply subsection in the Signal Descriptions section of the device-specific data sheet.
V1P8_SIGNAL_ENA bit is used to control the LDO output level used for controlling the SD card interface IO (signaling). The output of the LDO is connected to the processor IO supply group used for the SD card interface (VDDSHV5 for UHS-I speed support).
VDDSHV5 IO supply group for MMC1 was designed to support the power-up, power-down, or dynamic supply voltage change without any dependency on other supplies. This capability is required to support UHS-I speed.
Refer the Pin Connectivity Requirements section of the device-specific data sheet for connecting the LDO (SDIO_LDO) when not used.
For more details, refer to the Integrated Low-dropout Regulator (LDO) section in the Power chapter of the device-specific TRM.