SPRAD67B December 2022 – September 2024 AM2431 , AM2432 , AM2434 , AM6411 , AM6412 , AM6421 , AM6422 , AM6441 , AM6442
See the AM64x/AM243x DDR Board Design and Layout Guidelines. The goal of the guide is to simplify the DDR4 or LPDDR4 implementation. Requirements are captured as a set of layout (placement and routing) guidelines that allow board designers to successfully implement a robust design for the topologies supported by the processor. Any needed follow-up design support is provided only for board designs using DDR4 or LPDDR4 memories that follow the AM64x/AM243x DDR Board Design and Layout Guidelines.
See the AM64x/AM243x DDR Board Design and Layout Guidelines for the recommended impedance for the DDR4 or LPDDR4 signals.
For the propagation delay, the delay to be considered for DDR4 or LPDDR4 is the delay related to the traces on the board. If package level propagation delay is required, contact the local TI sales representative.
It is recommended to perform Signal Integrity (SI) simulations during board schematic design and layout stage.