SPRAD67B December 2022 – September 2024 AM2431 , AM2432 , AM2434 , AM6411 , AM6412 , AM6421 , AM6422 , AM6441 , AM6442
The DDR controller and DDR PHY have a large number of parameters to configure. To facilitate the configuration, an online tool (SysConfig tool) is provided that generates an output file that is consumed by the driver. Choose DDR Subsystem Register Configuration from the Software Product drop-down menu and choose the required processor. This tool takes board information, timing parameters from DDR device data sheet, and IO parameters as inputs and then outputs a header file that the driver uses to program the DDR controller and DDR PHY. The driver then initiates the full training sequence.
The SDK has an integrated configuration file for the memory (DDR4, LPDDR4) device mounted on the EVM or SK. If a configuration file is needed for a different memory (DDR4, LPDDR4) device, a new configuration file has to be generated using the DDR Register Configuration tool.
For more information, see [FAQ] AM62A7 or AM62A3 Custom board hardware design – Processor DDR Subsystem and Device Register configuration. This is a generic FAQ and can also be used for AM64x or AM243x family of processors.