SPRADB3A October 2023 – November 2024 AM2612 , AM2631 , AM2631-Q1 , AM2632 , AM2632-Q1 , AM2634 , AM2634-Q1 , AM263P4 , AM263P4-Q1
Table 9-1 contains a comprehensive list of Errata items from AM263 and outlines in which issues are fixed in either Rev 1.1 of AM263, Rev 1.0 of AM263P, or Rev 1.0 of AM261. Full details for the errata items are provided in the following documents:
Module | Description | Silicon Revisions Affected | |||
---|---|---|---|---|---|
AM263x | AM263P | AM261 | |||
1.0A | 1.1 | 1.0 | 1.0 | ||
ADC | i2346 — ADC result has error when switching between odd and even channels | Present | Fixed | Fixed | Fixed |
ADC | i2347 — VREF current consumption of ADC is random at power up | Present | Fixed | Fixed | Fixed |
ADC | i2349 — ADC VREFHI loading increased in power down | Present | Fixed | Fixed | Fixed |
AES | i2428 — AES in DTHE generates extra DMA request for data_in at the end of GCM encrypt | Present | Present | Present | Fixed |
BOOT | i2426 — ROM does not support OSPI extended OP Code in RDSFDP Sequence switching to 8S & 8D mode | Not Applicable | Not Applicable | Present | Fixed |
BUS SAFETY | i2393 — Granular error status not logged in BUS_SAFETY_ERR registers for the detected faults | Present | Present | Present | Fixed |
CLOCKS | i2324 — No synchronizer present between GCM and GCD status signals | Present | Present | Present | Present |
CONTROLSS | i2352 — CONTROLSS-SDFM: Dynamically changing threshold settings (LLT, HLT), filter type, or COSR settings trigger spurious Comparator Events | Present | Present | Present | Present |
CONTROLSS | i2353 — CONTROLSS-SDFM: Dynamically changing data filter settings (Such as Filter Type or DOSR) trigger spurious data acknowledge events | Present | Present | Present | Present |
CONTROLSS | i2354 — CONTROLSS-SDFM: Two back-to-back writes to SDCPARMx Register Bit Fields CEVT1SEL, CEVT2SEL, and HZEN within three SD-Modulator Clock Cycles can corrupt SDFM State Machine, resulting in spurious Comparator Events | Present | Present | Present | Present |
CONTROLSS | i2355 — CONTROLSS-ADC: DMA Read of stale result | Present | Present | Fixed | Fixed |
CONTROLSS | i2356 — CONTROLSS-ADC: Interrupts stop if INTxCONT (Continue-to-Interrupt Mode) is not set | Present | Present | Present | Present |
CONTROLSS | i2357 — CONTROLSS-ePWM: An ePWM Glitch can Occur if a Trip Remains Active at the End of the Blanking Window | Present | Present | Present | Present |
CONTROLSS | i2358 — CONTROLSS-ePWM: Trip Events are not filtered by the Blanking Window for the first 3 Cycles after the start of a Blanking | Present | Present | Present | Present |
CONTROLSS | i2359 — CONTROLSS-CMPSS:Prescaler counter behavior different from specification when DACSOURCE is made 0 or reconfigured as 1 | Present | Present | Present | Present |
CONTROLSS | i2405 — Race condition OUTPUT_XBAR and PWM_XBAR resulting in event miss | Present | Present | Present | Fixed |
CPSW | i2345 — :Ethernet Packet corruption occurs if CPDMA fetches a packet which spans across memory banks | Present | Present | Present | Present |
CPSW | i2401 — Host Timestamps cause CPSW port to lock up | Present | Present | Present | Fixed |
CPSW | i2402 — Ethernet to Host Checksum Offload does not work | Present | Present | Fixed | Fixed |
CPSW | i2329 — MDIO interface corruption (CPSW and PRU-ICSS) | Present | Fixed | Fixed | Fixed |
CPSW | i2438 — Host to Ethernet Checksum generation with VLAN ADD/Remove | Present | Present | Present | Fixed |
CPSW | i2439 — Host to Ethernet Timestamp accuracy issue | Present | Present | Present | Present |
CPSW | i2440 — Host to Ethernet Timestamp Sequence ID issue | Not Applicable | Not Applicable | Not Applicable | Present |
CRC | i2386 — CRC 8-bit data width and CRC8-SAE-J1850 and CRC8-H2F possible use in CAN module is not supported | Present | Present | Fixed | Fixed |
DCC | i2395 — DCC Module Frequency Comparison can Report Erroneous Results | Present | Present | Not Applicable | Not Applicable |
GPMC | i2313 — Sub-32-bit read issue with NAND and FPGA/FIFO | Present | Present | Not Applicable | Fixed |
ICSS | i2433 — Reading the 64-bit IEP timer does not have a lock MSW logic when LSW is read | Present | Present | Present | Present |
M4 ROM | i2403 — SBL redundant boot image feature not supported on HSSE devices | Not Applicable | Present | Present | Fixed |
MBOX | i2404 — Race condition in mailbox registers resulting in events miss | Present | Present | Present | Fixed |
McSPI | i2350 — McSPI data transfer using EDMA in ‘ABSYNC’ mode stops after 32 bits transfer | Present | Present | Fixed | Fixed |
OSPI | i2189 — Controller PHY Tuning Algorithm | Not Applicable | Not Applicable | Present | Present |
OSPI | i2351 — Direct Access Controller (DAC) does not support Continuous Read mode with NAND Flash | Not Applicable | Not Applicable | Present | Present |
OSPI | i2383 — 2-byte address is not supported in PHY DDR mode | Not Applicable | Not Applicable | Present | Present |
QSPI | i2364 — Access to address beyond 8MB is not supported in mem map mode | Present | Present | New OSPI module can support addresses beyond 8MB | New OSPI module can support addresses beyond 8MB |
R5FSS | i2374 — PBIST fails if clock frequency of R5SS_CORE_CLK is not same as R5FSS_CLK_SELECTED frequency | Present | Present | Present | Present |
ROM | i2426 — ROM does not support OSPI 8D boot mode for the flashes supporting extended opcode | Not Applicable | Not Applicable | Present | Fixed |
RAM SEC | i2427 — RAM SEC can cause Spurious RAM writes resulting in L2 & MBOX memory corruption | ||||
SDFM | i2375 — SDFM module event flags (SDIFLG.FLTx_FLG_CEVTx) do not get set again if the comparator event is still active and digital filter path (using SDCOMPxCTL.CEVTxDIGFILTSEL) is being selected | Present | Present | Fixed | Fixed |
SOC CONTROL | i2392 — Race condition in mem-init capture registers resulting in events miss | Present | Present | Present | Fixed |
SOC CONTROL | i2394 — Race condition in interrupt and error aggregator capture registers resulting in events miss | Present | Present | Present | Fixed |
TCM | i2411 — 128 Bytes burst access is not supported for TCM | Not Applicable | Not Applicable | Not Applicable | Present |
UART | i2310 — Erroneous triggering of timeout interrupt | Present | Present | Present | Present |
UART | i2311 — Spurious DMA Interrupts | Present | Present | Present | Present |
USB | i2412 — USB can not generate interrupt upon DMA read/Write Access error | Not Applicable | Not Applicable | Not Applicable | Present |
VDDA | i2348 — VDDA1V8 Static Power leakage | Present | Fixed | Fixed | Fixed |