SPRADC1 june 2023 DRA829J , DRA829J-Q1 , DRA829V , DRA829V-Q1 , TDA4VM , TDA4VM-Q1
The MSRAM block provides a memory mapped region that may be used to store various types of information. It uses a higher transaction issue rate bus interface with full support for multiple outstanding transactions and simultaneous completions of read and write transactions. For more information, see the Navigator Subsystem (NAVSS) chapter of the device-specific TRM
There are two MSRAMs on the device: 512 KB sized in the Main Domain (MSRAM16KX256E0_RAM) and the other of size 1 MB in the MCU Domain (MCU_MSRAM_1MB0_RAM).