SPRADC1 june 2023 DRA829J , DRA829V , TDA4VM
DDR is a shared resource between all the cores (R5F, M3, C6x, C7x, A72) in the system and needs to be partitioned for usage from different cores.
DDR usage:
To understand the system memory map in case of the vision_apps + Linux/QNX use case, see this developer note. A System generated memory map can also be seen in an autogenerated file at path: vision_apps/platform/j721e/rtos/system_memory_map.html
DDR memory ranges being used for RTOS firmwares should be non-overlapping with each other and should also be reserved from the HLOS side.
If DDR region used for MAIN R5F (say) is not reserved from HLOS, then the HLOS can use that space leading to memory corruption, as the MAIN R5F Software is running with the understanding that the DDR memory range is dedicated for its use.