SPRADC9 july 2023 AM62A3 , AM62A7
A defect detection systems is used to inspect products and detect abnormalities such as irregular shape, broken part, cracks, and so forth. It feeds information to a filtering system (for example, robotic arm) to separate units that are not accepted for packaging or for the following production processes. Depending on the types of the products and the expected defects, various types of input can be used including camera, laser, ultrasound, and so forth. This demo focuses on vision-based inputs. A typical defect detection system consists of the following components:
Using deep learning to process the vision-based input in defect detection systems has several advantages over using conventional machine vision algorithms. The next section presents a detailed comparison between the two options.