SPRADD2 august 2023 AM62A1-Q1 , AM62A3 , AM62A3-Q1 , AM62A7 , AM62A7-Q1
An extension of the DMS/OMS application is the need to provide eye safety by providing proper control of LED illumination. ASIL-B is typical safety integrity level targeted for this application. The software driver code that controls the LED via the LED driver is expected to run on the Cortex-R5 MCU. Safety mechanisms listed in Table 8-1 for MCU domain will be leveraged to provide protection of software driver code running on the Cortex-R5. LED driver shown in the diagram is an external component provided by system integrator. This LED driver can be functional safety qualified as well. Faults from the LED driver can then be further reported to the MCU R5. Software running on the Cortex-R5 MCU can take necessary action when faults are reported from external components such as the LED driver (GPIO can be used for fault communication) or internal fault reporting from error signal monitors within the AM62A device.