Python is only required for flashing files
or booting applications to the on-board EVM Flash via UART in the SDK. Below are the
steps for installation:
For Windows
- Download the latest version of
Python: www.python.org/downloads/windows/.
- Confirm Python is installed by
running the below command in command
prompt:
C:\> python --version
- If the command does not
return "Python 3.x", follow the link for more information: MCU+ SDK Python3.
- Check if the python package manager
"pip" is installed by running the below
command:
C:\> python -m pip --version
- Install below additional packages via
"pip" that are needed for the flashing tools (If proxy not needed, leave
blank):
C:\> python -m pip install pyserial xmodem tqdm --proxy={your proxy server web-link and port}
For Linux
- Run the below command in Linux bash
shell:
$ sudo apt install python3 python3-pip
- Check that if python package manager
"pip" is installed:
$ pip3 --version
- Install below additional packages via
"pip" that are needed for flashing tools (If proxy not needed, leave
blank):
$ pip3 install pyserial xmodem tqdm --proxy={your proxy server web-link and port}