SPRADF9
January 2024
AM263P4
,
AM263P4-Q1
1
Abstract
Trademarks
1
Control Card Overview
2
SDK and Dependencies
2.1
Software Development Kit
2.2
Python
2.3
OpenSSL
3
Code Composer Studio
3.1
Download/Install
4
Power Connections
4.1
Hardware Setup
5
Build and Run Example
5.1
Device Setup
5.1.1
Configure the Device's BOOT Mode to be Used With CCS Scripting
5.1.2
Setup UART Terminal
5.2
Example Project Setup
6
References
5.1.1
Configure the Device's BOOT Mode to be Used With CCS Scripting
Locate SW6 switches on the control card.
Change the switches to NO BOOTMODE [ 1 : 4 ] = 1 1 0 1:
Use
Figure 5-1
for reference.
Figure 5-1
NO BOOTMODE Switch
Press SW10 (PORz) and see red LED (LD19) toggle.