The reference design is set up with
the following elements:
- One TIDM-02009 DCDC converter
power board
The following list shows the key
resources used for controlling the power stage on the MCU:
- Two TIDM-02009 gate driver
card
- One TMDSCNCD263 controlCARD
- One 5V, 3A Raspberry Pi
adapter
- Mini USB cable
- Computer for loading software to
the AM263x MCU
The following list of test equipment
is required to power and evaluate the design:
- 15V, 4A bench-style supply for
primary board power
For DCDC converter Mode:
- 250W DC electronics load
- 1000V, 5A, 5kW power supply for
HVDC link input
- Oscilloscope with current and
high-voltage probes