Without purchasing a CODESYS License for the
CODESYS Runtime system on the EtherCAT controller, the EtherCAT network only
runs in Demo mode
Running in Demo mode means that fieldbus devices
such as EtherCAT devices terminate at 30 minutes
As of December 2023, CODESYS has migrated to a
new way of licensing across different hardware platforms. The new licenses are
Application Based Licenses
A quick method to check if the application is
running in Demo mode is if there is an orange cycle symbol next to
"EtherCAT_Master (EtherCAT_Master)" device in the device tree
Figure 8-1 CODESYS Demo Mode
Symbol
If the application is running with a license a
green cycle symbol is shown
Figure 8-2 CODESYS Licensed Mode
Symbol
Note that the CODESYS Development System that
runs on the Windows PC for GUI purposes does not require a CODESYS license