SPRADH9 June 2024 AM6442
S.No. | Test Specification |
---|---|
1 |
Description: Test to verify if desired PCIe vendor ID, device ID, subsystem ID & subsystem vendor ID can be set and configured correctly in the TMDS243EVM PCIe EP. Execution:
|
2 |
Description: Test to verify if a desired PCIe class code, sub-class code, the programming interface & the revision-ID can be set and configured correctly in the PCIe EP. Just for testing purposes the base class code needs to be set as “Input device (09h)” with a sub-class code set as “Gameport controller (10h)” and a programming interface set to “10h”. The revision ID is set to “03h”. For additional information regarding the encoding of above parameter refer to “PCI Code and ID Assignment Specification” as published by PCI-SIG. Execution:
|