SPRADH9 June 2024 AM6442
Description:
Test to verify if several PCIe outbound ATU configurations work correctly for the TMDS243EVM/TMDS64EVM PCIe EP.
The pcie_enumerate_ep application implements two outbound mappings. The first realizes a DMA mapping from internal “PCIE0_DAT0” window to a corresponding PCIe address. This DMA outbound mapping is used to write back received data from the RC. The second serves the MSI mechanism and maps the local MSI address configured by the RC to a corresponding PCIe address.
Execution: