SPRADH9 June 2024 AM6442
A root complex is the interface between the system CPU, memory, and the remainder of the PCIe interface. The root complex is either integrated into the CPU directly, or is external to the CPU as a discrete component. This interface also acts as a single source where all the data from various PCIe endpoints pass through. Figure 2-1 shows the root complex as the dark blue box that connects CPU, memory, and PCIe components and is referred as Root Complex.
For more details AM64x as RC