Test to verify if the Function Level
Reset (FLR) mechanism is disabled correctly at TMDS243EVM/TMDS64EVM PCIe EP.
Execution:
On Linux-based RC hardware, check
if the FLR mechanism is disabled at the PCIe EP. This can be checked at the
device capabilities as shown in the following figure