SPRADI0A July 2024 – November 2024
One of the key challenges while using model-based design is to generate optimized code for the C2000 MCU. While generating the code using C2000 Microcontroller Blockset, there are two stages of optimizations in use – Simulink tool optimization and C2000 specific optimizations. To generate the most optimal code for the application, each of the mentioned optimization needs to be configured. It is to be noted that, while we discussed about the TIDM-02012 eCompressor application in the previous section, the optimization settings that are discussed here are generic and can be applied for efficient code generation for all applications.